Part Number: BQ78350-R2-DEVICE-FW
Setting a Hex value of 0x230 in the Mfg status Init configuration does not seem to have an effect. Would like to keep the LED_EN, LF_EN and FET_EN Bits set in the .GG file, such that we do not have to use commands or BQStudio to toggle these bit states. Even though the GG file has 0x230 for this setting, the respective Bits do not turn ON, any reason for this? The only way these Bits turn ON is using BQstudio or sending the commands.