Other Parts Discussed in Thread: LM3578A
Hi
i have a system that the input voltage can be between 20-2V and I need to convert it to 2-6V.
the thing is that sometime the input is 2V and I need to convert it to 6V and sometimes the input is 20V and i need to convert it to 2V so the ranges are pretty big.
I need a component that can be a step up when needed and also a step down when needed and the output voltage should be adjustable between 2-6V.
is there such a component?
thanks in advanced.