Hi, I have two questions for this device:
1. Will the device reset when Vbus falls below VBUS_UVLOZ and then rises above VBUS_UVLOZ when the battery is 4.2V and always connected to VBAT?
2. For relative VINDPM, when VINDPM_OS is 600mV default value, I plug in a 6V adaptor, the VINDPM will be (6-0.6)=5.4V, correct?
If VBAT connected to a 4.2V battery, and I unplug the 6V adaptor and plug in a 5V adaptor, VINDPM will still be 5.4V or it will be updated to (5-0.6)= 4.4V automatically?