This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54335A: TPS54335A Question, UVLO measurement different from the calculation result.

Part Number: TPS54335A


Dear support member,

My customer used TPS54335A.
I have a question about UVLO.

(Situation)
R1(VIN - ENpin):430kΩ
R2(EN pin -GND):33kΩ

Calculated of Datasheet
Vsart:17.3V
Vstop:13.5V

Measurement result
Vsart:17.3V
Vstop:12.5V


(Question)
When the input voltage is 12.5 V, the output voltage is turned off.
It is different from the calculation result. (Vstop: 13.5 V)
What is the cause?


Best regard.
Bob Lee.