Part Number: TPS63020
Other Parts Discussed in Thread: ADS1256
Hi,
This is in regards with TPS63020 Buck-Boost regulator, we are facing an unique issue with the regulator. Our system is battery powered based on MSP432E microcontroller for water quality management. Measuring pH, Temp, Conductivity and Turbidity. We are powering section by section the circuit for measurement. When we are measuring the conductivity there is drop in the output voltage as shown in the datasheet when the device is configured for Power Save mode, but the device is not configured in power save mode. We initially thought it was the ADC ADS1256 which is creating the problem, based on TI Engineer suggestions we removed a lot of capacitors on the board, there was an improvement but not completely solved.
Please note the output voltage is set to 3.3V, MSP432E has an operating voltage of 2.97V to 3.6V, hence during the conductivity measurement the voltage drops as specifically when the PWM is switched ON or OFF for measurement. Link below explains the conductivity operations, In reference with the below circuit +15V & -15Vdc is generated using TPS65131RGER.
Another point to note: If 3.3V is supplied from an external source e.g. MSP432E Launchpad, everything works fine and there is no drop in the voltage, not even 0.1V on the 3,3V rail.
The layout is followed as per recommendation on the datasheet.
Kindly let us know how we could resolve the issue.
Regards,
Muruga