Tool/software: Linux
Dear TI support members,
Sub Commands "FG_SUBCMD_EXIT_CFGMODE = 0x0043" is defined in the following C source file
But, There seems to be no description in the Technical Reference Manual
Literature Number: SLUUBB0 December 2015
http://www.ti.com/lit/ug/sluubb0/sluubb0.pdf
I would like to see if the following is recognized about the effect of this Sub Commands (0x0043)
・Clear CFGUPMODE bit of Flags ()
・Set SS bit of CONTROL_STATUS
Regards,
Kazumi Kitano