Part Number: TPS7A78
Regarding TPS7A78, I see in the datasheet that the highlighted input voltage range is 70 to 270VAC. I understand that Cs and Rs affect the maximum AC supply voltage, so:
- Can this device support 347 to 480VAC input with a specific Cs/Rs configuration?
- On the other end, can it support 24VAC input?
- If so, in either case, is there anything to be aware of regarding the performance/capabilities of the device?
Thanks,
Brian