This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210: VBP in case of VDD=6~8V

Part Number: TPS40210

Hi all

Would you mind if we ask TPS40210?

There is the description on the datasheet P13;
"If the voltage at the VDD pin is less than 8 V, the voltage on the BP pin will also be less and the gate drive voltage to the external FET is reduced from the nominal 8 V."

Our customer will use TPS40210 with VDD=6~8V.

How much is the VBP in case of VDD=6~8V?
And how much is the internal LDO's VDO(drop voltage)?

Kind regards,

Hirotaka Matsumoto