Part Number: BQ51050B
Hi!
Here is my schematic for bq51050B.
Please check my schematic!!
I do not use LED to see whether it is charging. I use LCD screen instead.
I do not use a temperature sensor and TERM.
I just want 500mA charging current as a maximum.
The issue is about EN2 pin connection. I want it to be HIGH all the time because I do not have wired power source.
In its evaluation board (BQ51050BEVM-764), the EN2 is wired to RECT but the components connected to RECT are different now.
Can R16(1.5K ohm) be used? BQ51050BEVM-764 uses 1K in the RECT line.