This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25883EVM: Can BQ25883EVM operate alone without EV2400?

Part Number: BQ25883EVM
Other Parts Discussed in Thread: EV2400, , BQ25883, BQ25886

Hi TI,

I have customer want to evaluate BQ25883EVM, However he does not have EV2400 connect to PC. Can BQ25883EVM operate alone such as setting the hardware inside? If Yes, how to operate the devices?

  • Hello Yang OOi,
    The BQ25883 is a I2C controlled charger, so it will need EV2400 to do the evaluation.

    If the customer would like to use a standalone device, then BQ25886 would be the right device. You can order the EVM on ti.com.

    What is the application/end equipment?