Other Parts Discussed in Thread: LM5118,
Solar panel specification: 200W,Peak-voltage:36Vdc, Peak-current:5.55A, open-circuit voltage: 42Vdc, short-circuit current: 6.11A
Lead-acid battery volume: 24V/55AH
Is it possible to use a buck-boost(such as LM5118) to stabilize voltage then input to BQ24650?