Part Number: UCC28780
Other Parts Discussed in Thread: UCC27712
Hi,
I am currently working on a Active Clamp DC-DC Flyback Converter based on UCC28780 and UCC27712. If I succeed we will use this topology and components in various designs. But I am struggling. When I power up the circuit, Vdd starts to go up and down between 10V and 18V. Meanwhile PWML sends a single pulse, waits a while (maybe 1 second) then sends another single pulse. What am I missing here? I have calculated all the components according to the equatins which are in the UCC28780 datasheet. Please help me out.
Here are the parameters:
Vin is in between 30V and 60V.
Vaux:15V, Vout1:36V, Vout2:18V, Vout3,Vout4 and Vout5:15V
Best Regards.