A customer of mine is evaluating the LMG5200 and trying to figure out the best dead time circuit with least temperature drift for LMG5200 - The input threshold specification for LMG5200 is over free air temperature range:
The Schmitt inverter buffer used in the EVM design has a more wide threshold over temperature:
Would it not be better to remove U4A and U4B in the EVM dead time circuit below, due to that the turn on/off threshold variation is less in LMG5200 than in the Schmitt inverter over temperature?
In the EVM, 4 Schmitt inverters are used to generate the dead time? Is this necessary?