This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8758-E0: improve output noise

Part Number: LP8758-E0


Hi,

My customer is using LP8758-E0 to supply PLL in 400Gbps optical module. They need to minimize the switching noise of output voltage to achieve better eye diagram. I've suggested adding a snubber at switching node and optimizing the layout.I would like to confirm two questions,

1. Is there any register that can reduce the slew rate of switching on and off?

2. Does the parasitic capacitance of the inductor couple noise from switching node to output? So should I also choose a low parasitic capacitance inductor?

You could suggest any other measure to reduce the output noise.

Thanks.

  • Hi Jerry,

    Snubbers can help with switching spikes if they are correctly tuned. But for sure the layout is most important.

    1. No.

    2. That is possible. Depends the inductor type etc. things. But my suggestion is to first to focus output capacitors and check if those can be modified or added more with different values and low ESL type.