Other Parts Discussed in Thread: TPA3255, UCC28C45, UCC2897A, UCC3808-1, TL431
Dear Team
I am beginning to develop an LLC DC-DC converter using the UCC256301.
My input voltage is 12v (10-12v)
Output voltage will be 53v as I'm intending to use this with a TPA3255 audio amplifier in a 'portable' application, so I'm seeking the best possible efficiency.
I realize that I have to alter a number of values/parts to facilitate the 10-12 v DC input operation, but the spec sheet seems to suggest this is possible within the range of input values required for the various functions.
As I look at the suggested application information, I find myself a tad confused on the matter of calculating the feedback resistor values.
In the AC/DC schematic it shows a number of oddly valued resistors that probably only exist in some parallel universe. (See Image)
I don't need isolation in this application due to the low voltages involved.
QUESTIONS.
Is there a simple alternative cct which does not require the use of the OPTO coupler and the TLV reg (as per image) ?
I obtained the feedback arrangement directly from the EVM schematic, but that has 12v o/p and I have 53v.
If this is feasible, can I get some assistance with such a feedback arrangement and some values ?
Web Bench will not allow <30v DC input so I can't resort to that for design help.
Thanks
Julian de Ross