This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLK / RT mode change

Other Parts Discussed in Thread: TPS54320, TPS54310, TPS54350, TPS54824, TPS54424, TLV62130

Dear all.

The following comments are written in datasheet of TPS54320;
"TI does not recommend to switch from the CLK mode back to the RT mode, because the internal switching frequency drops to 100 kHz first before returning to the switching frequency set by RT resistor."
Is there the device which such a phenomenon does not occur even if we change a mode?

VIN=8.4V(2cell)

VOUT=4.5V
IOUT=1A to 3A

Regards,
PAN-M