Other Parts Discussed in Thread: BQSTUDIO
Dear Technicians:
My product is 48v16ah. After setting the voltage divider network (VOLSET set) voltage divider to set 58800mv, the voltage read by bq software is only about 42v, and the actual battery pack voltage is 47v.
1. I have entered 47v in the calibration voltage interface, prompting me to exceed the voltage range. How to solve it? Can I manually adjust the value of the Voltage Divider to calibrate to the actual voltage?
2, my battery pack is 14 strings, is the Number of Series Cells set to 14?
3. Does Design Capacity mean single or single string, or the capacity of the entire battery pack?
4. Does Design Energy mean a single or a single string, or the energy of the entire battery pack?
5. Is Number of Series Cells in multiples with certain parameters? such as?