This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Some problm about Tps25982

Part Number: TPS25982
1. My normal working voltage is 3.3V, can provide overvoltage protection 3.7V

2. How to understand active current limiting and circuit breakers

4. Why can the package be able to do this small, the same load area of the ADI is several times that of yours, and how to ensure the cooling of this small package

5. There is usually a current sense resistor. I see that this device has been canceled. What method is used instead of the function of this resistor?

6.Tps25982 mass production time?