Other Parts Discussed in Thread: BQ51050B
Hi,
As described in the related thread created previously, we are using battery protection IC bq29700 to protect 210mAh Li-Ion battery PGEB014461. When the battery voltage is drained below 2.8V, battery over discharge status is detected and battery is getting disconnected from further loading. When the charger is connected the over discharge status is never getting released and therefore battery is not at all charging. Actually battery is charging in the over discharge detection delay time 144ms only. In the previous thread we didn't got any solution for this issue. Once the battery is very slowly charged above 2.85V or 2.9V with the help of 144ms interval, we need to short the battery negative terminal and module to ground to initiate proper charging. As an end product this won't be good for us. Kindly help for finding a solution for this. Why bq29700 is not properly detecting that a charger is connected to charge the battery so that it should release over discharge state.
Note: Battery charger charge current is between 160mA to 210mA.
Regards
Hafiz