This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24715: BQ24715 Leakage current when os is idle without heavy loadings

Part Number: BQ24715

HI,

we use BQ24715 for nvdc Charge soulution, battery will drop its RSOC from 100% to 97% when OS is idle without heavy loading at two hours.

test the discharge Mosfet, the Gate open random and last on 2~4ms. as this condition ,the battery RSOC drop

check the  register  without change.

would you please confirm why the charge ic discharge or the  charge IC could not latch the discharge mosfet continuelly.

fordring.wang

18664983545

  • Hi,

    Based on your description, it sounds like your system is occasionally drawing >256 mA of discharge current from the battery. This will cause the BATFET to turn on, as described in Section 8.3.12 of the datasheet.

    To confirm whether this is the case, you could try probing BATDRV and ISYS and see if the times when BATFET turns on correspond to times of higher current being drawn by the system load.

    Best regards,
    Angelo