Hi,
We are seeing some strange behaviour around the TPS3852 in our circuit.
We are using feedback on the SET1 pin to enable and disable the watchdog. We have seen that disabling via SET1 during an active WDO event, terminated the event. This was as described in a previous answer.
However, we are also seeing that under certain conditions the RESET output is also shortened and not the standard 200ms duration.
Can you confirm if this is possible and what is the mechanism?
Thanks Pete