Tool/software: Linux
Is there any update on a LP5018/5024 Linux driver? I see that you were working on it back in December.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Is there any update on a LP5018/5024 Linux driver? I see that you were working on it back in December.
Thanks Kenneth. When I load the driver, and then the I2C device, with the commands below, I'm getting an error "LEDs are not defined in device tree!"
insmod /lib/modules/4.14.39-v7/kernel/drivers/leds/leds-lp50xx.ko
echo lp5018 0x28 > /sys/class/i2c-adapter/i2c-0/new_device
I see this is an error from the driver source. What do I need to do to resolve this, is there a step I'm missing?