Other Parts Discussed in Thread: BQ25713, BQ77915, PMP40441
Dear colleagues,
I am working on a smart speaker project where we need to use battery+BMS powered by USB-C PD.
We identified the BQ25713 which seems a good circuit for such application. Combined with 3S battery @ approx 4Ah.
Use case 1: speaker is connected to USB supply. The product will need 20V output to operate correctly.
Question1: How do we configure USB-PD charger to send 20V instead of 5V ? ideally with a stand-alone circuit instead of a copy-pasted obscure chunk of soft on a µC.
Question2: Is it OK to connect the system directly to VBUS, instead of VSYS ? Is it OK to not use VSYS or does it needs some load ?
Use case 2: The battery is charged and the user disconnect the charger. The speaker needs to stay ON during the transition.
Question3: Is OTG fast enough to maintain VBUS at 20V and keep device ON ? Is there a minimum capacity value needed ?
Use case 3: Speaker runs on battery. Because the speaker circuits needs 20V and 3S Li-ion is only 3*3.7V = 11V, we need to boost it up. This is why we want to connect the system to VBUS.
Question4: Correct me if i am wrong but in battery mode, VSYS can only go as high as battery voltage, right ?
Question5: Overall, is such a concept a good usage of the BQ25713 circuit or not ?
Use case 4: Speaker runs on battery and user decides to connect back the charger.
Question6: Is it safe for both the charger and BQ25713 or do wee need to put a PMOS switch in between ?
Question7: Also, in PMP40441 ref design (buck-boost USB-PD charger) we see a BQ77915 circuit for cell protection. Do you recommend using it or we can use BQ25713 only ?
Thank you guys in advance for your help.
Best regards,
Samir