This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3831: P2P Direct Replace

Part Number: TPS3831

Dear Team,

Do we have a solution can directly replace here:

STM811SW16F

BR

Kevin

  • Kevin,

    We do not offer voltage supervisors in the SOT143-4 package. We have direct replacement for the SOT23-3 variant without the manual reset pin, and we have functionally equivalent device to the STM811 in the SOT143-4 package.

    TPS3831 is a good choice as a functionally equivalent and is actually a much better device. STM811 has Iq of 6uA typical compared to TPS3831 with typical Iq of 0.15uA.

    -Michael