This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ30Z554-R1: BQ30Z55 Can't turn on the CHG FET issue.

Part Number: BQ30Z554-R1
Other Parts Discussed in Thread: BQ30Z55

Hi sir,

     my customer is using BQ30Z55 for 2S battery pack ,now when they test the function, they find that if not connect the SMBUS, in charging mode , BQ30Z55 can't turn on the CHG Fet. it only can be active by connect the SMBUS or connect a load to discharge, the CHG FET can be turn on ,could you please help to suggest which setting will result this issue?

  • Hi Jerry

    Does the customer have a schematic that they can share? Can they provide log and gg files from the failing system? Is this a one off failure and do they have other functional units which they can use for comparison?

    Do they have an EVM which they can use as a reference to test their battery packs?

    thanks
    Onyx