This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60301: TPS60301

Part Number: TPS60301

I'm using TPS60301 for my application to generate 3v from 1.5v supply.

The charge pump is wired as provided in the datasheet, using five 1uF capacitors.

The enable pin is connected to the input pin.

Sometimes it is noticed that the input and enable pin indicate only 0.7v against the expected value of 1.5v, though power supply indicates 1.5v. once this problem occurs, it stays for a long time. If switched off for some time, the output comes back again. I'm using Out2 for my application.