Part Number: BQ24250
bq24250 battery charger, specifically the TS (NTC monitor) operation.
According to the datasheet, the pin has a TS disable threshold of 70% of LDO voltage.
As I understand it, it will continue to charge the battery if the TS voltage is above the threshold.
In a single-fault condition, with R2 shorted, the voltage will be above the threshold which will allow to charge the battery even if the battery temperature is too high.
Am I understanding this correctly? Is there a solution or a possible overwrite to the TS disable threshold?