This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: For EN/UVLO setup can i use a 750K ohm for RUV2 ?

Part Number: LM5175


Hi 

For EN/UVLO setup can i use a 750K ohm for RUV2 ? 

The datasheet did not mentioned the Max allowable resistance for RUV2. 

Thanks!

PY Tsai

  • Hi PYTsai,

    Theoretically the there is not a maximum resistance that can be used on the bottom UVLO resistor divider. However I don't recommend using a resistor that large due to the poor noise immunity.

    If the goal of the resistor is to set a large turn-on voltage and turn-off voltage hysteresis the it is better to place a resistor in series with the the UVLO pin to control the hysteresis.

    Please let me know if you have any questions.

    Thanks,

    Garrett