This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Taper current

Part Number: BQ27426

Hi TI support members,

The Quick-Start Guide for bq27426 Fuel Gauge (sluubn3) P3 states that "The Taper Rate value allows the gauge to synchronize its full charge detection point with that of the charger."

Does this mean that SOC = 100% when the charge current value measured by bq 27426 becomes taper current?

For example, I set it as follows.
-Taper Current: 60 + (60 * 0.1) = 66 (mA)
-Taper Rate: 800 / (0.1 * 66) = 133 (.1 Hr rate)

In this case, does it mean that SOC = 100% when the current value measured by bq 27426 reaches 66 mA?

Regards,

Chiaki Endo