Hello,
I'm facing the same problem as mentioned in the last thread.
Trying to create active shutter goggles with this specifications:
- Enable shuttering of each of the glasses lenses independently
- Enable both lenses to be open or shut simultaneously
- Once a shuttering command (open or close) has been sent to a lens, the lens shall remain at the same state until the opposite command is sent
As said in the last thread, this is not possible with the TPS65835. Could someone advise me another model, which would allow me to solve this problem?
An additional point is that my Shutter LCDs require 5V for complete darkness. In case this is imporatnt to descide for a model as well.
Best, Simon