Other Parts Discussed in Thread: BQSTUDIO, BQ76930
Hello team,
Currently my customer is testing out the BQ78350 paired with BQ76930 platform on the dev board using bqStudio. They are running into a bit of a challenge with the setup. They can't seem to setup the Data Memory so that the system allows current draw of more than 9A. The system keeps shutting down the FETs when it hits around 9A. The customer thinks they have turned off all the discharge protection that they can find, but still no dice. What are the settings needed to get past the 9A limitation?
Thank you for your support!
Errol
Texas Instruments
Field Applications Engineer