This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25150: comparison table for the

Part Number: BQ25150
Other Parts Discussed in Thread: BQ24074, BQ25606

Hi team,

Could you please help fill the blanks of the BQ25150 and the BQ24074 in the comparison table we did in below(or attached)?

We didn't see the parameters in the datasheet and need your help.

Also put the BQ25606 FYR since there are different structure.

Thank you! 

  • Zoe,

    My response is in below.

    1. Rdson

    BQ25150: 100mohm (typical) & 175mohm (max)

    BQ24074: 50mohm (typical) & 100mohm (max)

    2. Leakage current

    BQ25150: 1.7uA (typical) with LDO enable & low power mode

    BQ24074: 6.5uA (typical) with out system load condition

    3. Efficiency

    linear charger efficiency is simple, just Vout/Vin

    Thanks