This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti experts,
Below is from the datasheet of Lm3644, does it mean LM3644 can output 179ma maximum current in seperated channel at the same time ? Besides, when we combine the 2 channel, can it reach 179ma+179ma to driver 1 LED? Thanks a lot.
From datasheet:
In Torch mode, the LED current sources (LED1/2) provide 128 target current levels from 0.977 mA to 179 mA or 1.954 mA to 360 mA on LM3644TT