This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61194-Q1: how can I get more the 100mA output from TPS61194-Q1

Part Number: TPS61194-Q1

HI Sir,

the specification shows "Outputs can be Combined Externally for
Higher Current per String"

it that means combine the two outputs together can double the output current?

if I want to get 140mA how should I do,

please advise,

thanks!

with best regards,

Peter Zha