HI
My customer now wants to develop an inverter to operate a 30V UV lamp.
Is there an IC that can be recommended for inverter development of about 10W with input voltage of 12Vdc and output of 30V/0.3A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
thank you for your quick reply.
I'm not looking for boost ic ...;
inverter related solution.
The input voltage is DC 12V and the output voltage is AC 30V.
The inverter circuit using TI's CD4047 + ULN2004 was found on GOOGLE.
But the CD4047 is too old IC. Is there a solution to this?
Hello Andy,
I see the similar circuits you found on the web.
TI's archives do no yield any 30VAC output designs to fit your need.
What frequency and current are you needing to drive the UV LED?
10W with input voltage of 12Vdc and output of 30V/0.3A, is this RMS or peak current.
Can you provide the UV LED part number?
The CD4047 + ULN2004 combination is still a valid design, both devices are active and can be purchased.
www.ti.com/.../CD4047B
www.ti.com/.../ULN2004A
There are newer devices to replace these two.
CD4047B CMOS Low-Power Monostable/Astable Multivibrator
VCC max is 18V for this and some of the other CDxxxx devices.
Newer multivibrators have a lower VCC rating, ~6V
All TI Multivibrators may be found here:
www.ti.com/.../products.html
ULN2004 is a 50V, 500mA Darlington low side driver.
All TI low side switches may be found here:
www.ti.com/.../products.html
Suggested newer replacement is TPL7407L, 40V, 600mA low side NMOS driver
www.ti.com/.../description