Hello,
I need to build a solar charger for a LiFePO4 battery.
The requirements are to support 4,5,6 and 7 cells batteries.
Consulting the app note SLUA565 (Using the bq24650 to Charge LiFePO4 Battery), it is explained how to add a resistor in parallel to R23 (R15 in the app note) to reduce V_refcharge to 3.4V for example, however this app note address only 1 cell battery.
In order to support 4 to 7 cells, I need to do the following:
1. Change R22 (R13 in the app note) for each battery type assuming R23 (R15 in the app note) is constant.
So in my design, if R23 is 100K than for 5 cell R22 will be 757K and for 6 cells 928K and so on right?
2. Set the parallel resistor accordingly, 3M ohm looks like the correct value.
3. MOSFET - in this solution the gate of the MOSFET is connected to STAT2. Vsys in my design can be 28V so it will burn the gate. I see no reference to that in the app note. Will a zener diode make sense or am I missing something here?
Thanks,