Part Number: BQ34110
Other Parts Discussed in Thread: BQSTUDIO, , EV2400
Hi Team TI,
I'm working with a BQ34110 to monitor a 6000mAh 12.8v LiFePO4 battery pack. The pack contains 4 cells in total and They are configured as 4 series cells. I am using bqstudio and EV2400 to communicate.
The problem we are having in configuring the gauge to correctly monitor the remaining capacity and the Relative State of Charge(SOC). I have set up the Voltage Divider parameter, calibrated the voltage and current, and I am getting accurate readings for both Current and Voltage from the battery pack.
Q1. In bqstudio Design Capacity and Full Charge capacity is set to Default Value of 2200mAH. I need to change that to 6000mAH. Please suggest me how to configure these parameters.?
Q2. Also, Suggest me which are the other parameters I need to configure to get the accurate SOC.