Other Parts Discussed in Thread: TPS546C20
TPS546C20 Two Phase mode:
1,Can you work in a hardware-only way without PMBUS?
2,Since the PM_BUS feature is not used, protection functions such as OCP/OVP/UVP are implemented on external lines. Please also confirm what is the default OCP/OVP/UVP protection point within the IC and how to adjust it to avoid conflict with the protection point on the external line?