This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27411-G1: bq27411-g1: which offsets are correct, pdf or bqStudio

Part Number: BQ27411-G1
Other Parts Discussed in Thread: BQSTUDIO,

Hi,

According to Table 6-3 (bq27411-G1 Technical Reference SLUUAS7B) that describes subclass 80 (IT Cfg), parameters from "ResRelax Time" to "TermV Valid t" should have offsets 48-76. But bqStudio uses offsets 50-78 (+2) for them.

So the question is which offsets are correct?

There are also undocumented registers: "Qmax max delta %" and "Max % default Qmax" (exist in bqStudio but not in pdf), and documented register "Fast Qmax Volt buffer" that cannot be edited by the application.

Are they important for correctly working IT? If so, what values (and offsets) should they have?

Thanks