Tool/software: WEBENCH® Design Tools
Hi team,
My customer would like to set the mode as follows.
-Light load operation : FCCM
-Current Limit : ILIM
-Frequency : 1200kHz
According to the Table.3 in the d/s, Rml should be 51kohm and Rmh should be 180kohm. However, the Webench recommends Rml=49.9kohm and Rmh=158kohm. Is this an error of Webench?
/cfs-file/__key/communityserver-discussions-components-files/196/TPS56C215-WBDesign1107.pdf
Regards,
Yamaguchi