Part Number: LMR33630-Q1
Other Parts Discussed in Thread: LMR33630
Hi~
In LMR33630-Q1 datasheet, Fig.23 shows that max load current vs ambient current.
Even though consider Rtheta_JA=50dec/W(realistic PCB), max load current at 85deg is just about 2.2A.
Does it means LMR33630 cant cover at all up to 3A full load at 85deg condition?
Or is there any way to support 3A at 85deg by increasing copper or any other way?
(In Fig.22, even though use large copper area, Rtheta_Ja can't reduced below 48deg, so looks limitation.)
Thanks.