Other Parts Discussed in Thread: BQ25703, BQ25713
Hi,
the datasheet for the BQ25703A mentions that it's possible to set inductor values via a resistor and lists the possible resistor values for 1µH, 2.2µH and 3.3µH.
It doesn't mention the 1.5µH inductor, which as far as I can tell from other places in the datasheet is also supported. Should this one use the 1µH value instead?
"Recommend 800 kHz with 2.2 μH or 3.3 μH, and 1.2 MHz with 1 μH or 1.5 μH.
Host has to set the right PWM frequency after device POR." (p37)
Is there any formula to calculate the resistor value? As far as I can see this value is used to calculate the power consumption and the better it is matched to the inductor, the better the consumption could be calculated.
Thanks in advance,
BG