I’ve set my charge current to 2A for my BQ24616 design but the IC is outputting about 3A. The voltage VIset1 = 0.396V when there’s no battery connected. However, the voltage changes to 0.46V - 0.49V when a battery or load is connected. The 3.3V reference voltage for Iset1 does not change with or without load. I’d like your assistance in solving this issue.