This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27421-G1: hibernate mode

Part Number: BQ27421-G1

hello,

our customer is looking for a way to minimize bq27421 consumption current and he has a plan to utilize Hibernate mode. Could you please suggest if the gauging accuracy will be deteriorated by using Hibernate mode frequently.

best regards,

  • yes it will.
    if you cut off power you will need to have non volatile memory where you store data memory contents with your configuration so you can load it back on the gauge.

    thanks
    Onyx
  • Thank you. I understand the hibernate mode is effective for saving power if a customer store a NVM on outside.

    However, let me confirm one thing.

    Does this use case make getting worse the gauging accuracy?

    best regards,

  • You will loose passed charge data when you wake from shut down. the gauge will estimate SOC based on OCV measurement. This could be prone to errors if there is a current flow into or out of the gauge. So yes this will affect accuracy. However, Once you charge the device to full or discharge to empty which are reference points, the device will resume good accuracy.

    thanks
    Onyx
  • I mostly understand but want to know about "This could be prone to errors if there is a current flow into or out of the gauge." that you mentioned in detail. Does this case insist gauging accuracy is getting worse if any current flow into or out of gauge when the device is working in Hibernate mode ?
    best regards,
  • Hi Toshiro
    In hibernate, the gauge is pretty much non-fucntional. It is not coulomb counting. When it wakes up from hibernate, it takes an OCV measurement, performs a remcap simulation and estimates SOC. This estimation will have errors if you have current flow. We cannot determine how much error will exit as this is dependent on the amount of current. So if you continuously put the gauge in hibernate each time you wake, you will be prone to error until the device is charged to full or discharged to empty before good accuracy is restored. I hope this helps.


    thanks
    Onyx
  • Thank you very much. I understood.

    best regards,