Hi Team,
I received the following request:
#########################################
We have a problem with buck-boost dual converter TPS65131RGER. Our product has just started production but we could not solved it, it is very urgent.
The symptoms are below:
When the input voltage (marked as Battery_Out in the schematic) goes above 4.05V, both output stages of VR4 (TPS65131RGER) become unstable, i.e the 8V stage falls to about 3.8V and -5V stage even worse. The supply outputs are quite stable when “Battery_Out” ranges between 3V to 4.05V.
We checked the datasheet again but could not find any component value or related specification that seems wrong to cause such a behavior.
#########################################
I will send the schematic separately.
Regards,
Fabio