Other Parts Discussed in Thread: BQ76PL455A
Hi all,
i´m working on a system with two bq76pl455a-q1.
Device #0 is in bottom position, set to single communication mode and communicates with microcontroller via UART.
Device #2 is in top position and comm. mode ist set to differential, and communicates via daisy chain communication.
So far we can can wake up the devices, configure AFE, baudrate and so on.
Right now every 20 ms all the results are transmitted and evaluated by the micro.
The only thing we are struggling with is the power down procedure.
If we broadcast the power down command, only the bottom device, that is directly connected to the micro is going into shutdwon mode.
The green LED on EVM1402 is still glowing. It does not glow until it is wake up during power up procedure, but once it is glowing we found no other way to power down than
disconnecting the battery connector.
Help is appreciated how to power down