This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear support member,
My customer used TL431.
I have a question.
(Question1)
Is it possible to use two TL431 connected in series to make 2.495 × 2V?
(Question2)
If it make 2.495 × 2V possible,
could you teach if there is something like a recommended circuit?
Best regard.
Bob Lee.
Dear Trailokya Rai,
Thank you very much for reply.
May I ask a add question?
(Question)
Can I use two TL431s in series?
Best regard.
Bob Lee.
Dear Trailokya Rai,
Thank you very much for reply.
I mistook schematic.
The correct circuit diagram is following schematic.
May I ask add a question again?
(Question)
Q1.
My customer want to use following schematic.
Is there problem?
Q2.
Does the current change and cause problems such as oscillation?
(Specification condition)
Input:15V
Output:5V
Best regard.
Bob Lee.
Dear Trailokya Rai,
Thank you very much for reply.
There is question about your answer.
What mean "satisfy KCL"?
What mean "take extra care"?
Is there include any problems?
Best regard.
Bob Lee.
Dear Trailokya Rai,
Thank you very much for reply.
Is there a problem with a circuit diagram using the bottom resistor?
You mean there is a problem, right?
As TL431 controls the voltage by IKA,
Can control a circuit diagram using the bottom resistor?
Best regard.
Bob Lee.
Dear Trailokya Rai,
Thank you very much for reply.
May I ask add question?
How much is voltage variation of ZKA?
Althought I will return to the first question,
Can this circuit be guaranteed to operate stably at 5V output ?
Best regard.
Bob Lee.
Bob
ZKA < 0.5 ohm for TL431. The voltage variation will be very less. Both the scheme (With and without bottom resistance) will give you stable output.
Regards
Trailokya