Hello,
I have a couple of questions about BQ25713 input capacitor.
1) It looks that the EVM has 60uF of CERMs and 33uF of TA balk on the VIN line. If there is more capacitance(e.g. total 200uF), should it be acceptable case or is there any concern for larger input capacitor case. Some application may have a larger bulk cap on the VBUS input.
2) Can the 33uF of TA alter to CERM or E-caps as well?
Thanks in advance.
S.Sawamoto