Hi!
We've been trying to use the BQ24650 as the charger for a lead acid battery, as you can check on the schematic. We followed the slva437a application for a 1.6A charge current
Our voltages are as follow:
VCC: 23.97V
VFB: 1.8V
SRN: 12.73V
MPPSET: 1.54V
STAT1: 23V
STAT2: 17V
VTS: 1.9V
REGN: 6V
VREF: 3.29V
And this is what it looks like on the battery side:
Could you please help us?