This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: VBST current

Part Number: TPS53355

I want to know the average value of VBST current .  I want to add a resistance between VBST and LL.  Can I  use 0402 package ?

  • User,

    I doubt that we have that data. The absolute maximum rating is 50 mA. Typical may be in the range of 10 mA. If you want to use a series resistor, I recommend 2 ohms.  0402 is ok to use.  Make sure to include the recommended BST capacitor. 0.1 uF, in series.